Adding HDMI in i.MX8M Mini U-Boot - Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding HDMI in i.MX8M Mini U-Boot - Yocto

1,189 次查看
kanimozhi_t
Contributor V

    I'm building Yocto's warrior core-image-base for i.MX 8MM and sound that the produced U-Boot is void of HDMI component.

    I want to build U-Boot with HDMI so any help in enabling HDMI in the build would be appreciated.

Thanks in advance.

0 项奖励
回复
1 回复

1,096 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kanimozhi

in uboot one can try to enable ADV7535 (MIPI-DSI to HDMI converter)

imx8mm_evk.c\imx8mm_evk\freescale\board - uboot-imx - i.MX U-Boot 

i.MX8M Mini has not HDMI block as described in AN12296

i.MX 8M Mini Migration Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复