Adding HDMI in i.MX8M Mini U-Boot - Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding HDMI in i.MX8M Mini U-Boot - Yocto

1,189件の閲覧回数
kanimozhi_t
Contributor V

    I'm building Yocto's warrior core-image-base for i.MX 8MM and sound that the produced U-Boot is void of HDMI component.

    I want to build U-Boot with HDMI so any help in enabling HDMI in the build would be appreciated.

Thanks in advance.

0 件の賞賛
返信
1 返信

1,096件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kanimozhi

in uboot one can try to enable ADV7535 (MIPI-DSI to HDMI converter)

imx8mm_evk.c\imx8mm_evk\freescale\board - uboot-imx - i.MX U-Boot 

i.MX8M Mini has not HDMI block as described in AN12296

i.MX 8M Mini Migration Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信