Dear all,
I check VIN of SW2 of PF0100.
I checked Absolute Maximum Ratings of the PF0100 data sheet.
- Table 5. Absolute Maximum Ratings(P.11)
Furthermore, I checked the following point.
- SW2 Specifications(P.63)
However, I was not able to find a description of VINSW2.
I found Max Rating in Pin Definitions.
- Table 4. PF0100 Pin Definitions(P.9)
Should I refer to this Tabel 4 as Absolute Maximum Ratings for VINSW2?
(In this case I do not understand the minimum value.)
Best Regards,
Yuuki
Solved! Go to Solution.
Hi Yuuki
based on Table 4,5 Absolute Maximum Ratings
are -0.3 to 4.8V.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuuki
based on Table 4,5 Absolute Maximum Ratings
are -0.3 to 4.8V.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------