Absolute Maximum Ratings for VINSW2 of PF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Absolute Maximum Ratings for VINSW2 of PF0100

Jump to solution
721 Views
yuuki
Senior Contributor II

Dear all,

I check VIN of SW2 of PF0100.

I checked Absolute Maximum Ratings of the PF0100 data sheet.
- Table 5. Absolute Maximum Ratings(P.11)

Furthermore, I checked the following point.
- SW2 Specifications(P.63)

However, I was not able to find a description of VINSW2.

I found Max Rating in Pin Definitions.
- Table 4. PF0100 Pin Definitions(P.9)

Should I refer to this Tabel 4 as Absolute Maximum Ratings for VINSW2?
(In this case I do not understand the minimum value.)

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
657 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

based on Table 4,5  Absolute Maximum Ratings

are -0.3 to 4.8V.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
658 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

based on Table 4,5  Absolute Maximum Ratings

are -0.3 to 4.8V.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply