Dear all,
We want to run DDR Stress Tester on the our original iMX6DL board.
However, in our board, USB_OTG is not implemented.
And, SD3_DAT6/ALT1(RX) and SD3_DAT7/ALT1(TX) are used as UART1.
DDR_Stress_Tester_V1.0.2_UART1_for_SDboot&JTAG.zip uses CSI0_DAT10/ALT3 and CSI0_DAT11/ALT3 as UART1.
It is necessary for us to modify it to use following pins of UART1.
- RX:SD3_DAT6/ALT1
- TX:SD3_DAT7/ALT1
Therefore, I got a source code of the DDR_Stress_Tester_V1.0.2.zip from FSL local FAE.
For UART1 pins, we made the following modifications.
iMX6_DDR_Stress_Tester_source\src\mx6dlのhardware.c
[Before]
#elif UART1_1
/* UART1 TXD */
writel(ALT3, IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT10);
/* UART1 RXD */
writel(ALT3, IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT11);
// daisy chain setup
writel(0x1, IOMUXC_UART1_IPP_UART_RXD_MUX_SELECT_INPUT);
[After]
#elif UART1_1
/* UART1 TXD */
writel(ALT1, IOMUXC_SW_MUX_CTL_PAD_SD3_DAT7);
/* UART1 RXD */
writel(ALT1, IOMUXC_SW_MUX_CTL_PAD_SD3_DAT6);
// daisy chain setup
writel(0x11, IOMUXC_UART1_IPP_UART_RXD_MUX_SELECT_INPUT);
DDR_Stress_Tester_V1.0.2.zip uses USB_OTG port.
It is necessary for us to switch from USBOTG to UART1.
Would you teach a modification file and the contents to change from USB_OTG to UART1?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi Yuuki
please follow recommendation on link below in case when USB_OTG is not available:
If USB OTG port is not available on customer board, please use the images in
DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG.zip.
The bin files in the packages can be loaded by uboot and elf files are used by JTAG load.
i.MX6 DDR Stress Test Tool V1.0.3
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor-san,
Thank you for your quick response.
The DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG image uses CSI0_DAT10 pin and CSI0_DAT11 pin for UART1.
In customer board, UART1 is assigned SD3_DAT7 pin and SD3_DAT6 pin.
Therefore we cannot use DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG.
It is necessary for us to modify a source code of DDR_Stress_Tester_V1 .0.2.
We understood the method to set pins of UART1.
However, we do not understand a method to change from USB-OTG to UART1.
Would you teach this method?
Or, would you send it to me if there is a source code of DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG?
Best Regards,
Yuuki
Hi Yuuki
there is no "method to change from USB-OTG to UART1"
since iROM uses SDP for loading image - it uses only USB OTG,
it can not be changed to UART: this is hardware limitation.
So one needs to use JTAG.
Best regards
igor
Dear Igor-san.
Thank you for your response.
I suppose that DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG binary image is made by DDR_Stress_Tester_V1 .0.3 source code.
Would you teach the change point when DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG was made?
Best Regards,
Yuuki
Hi Yuuki
there are no changes, just follow "MX6_DRAM_Stress_Test_Guide_vx.pdf"
whch is included in DDR_Stress_Tester package p.12:
..This creates the DRAM Stress Test images (.bin and .elf files) under the directory
.\dram_stress_test\output\mx6x\bin (Note that a new directory .\dram_stress_test\output has been created)
6. The .elf file can be used with a JTAG debugger
also please follow this document sect.5 How to run the DRAM Stress Test from the debugger
Best regards
igor
Dear Igor-san,
Thank you for your support.
I do not have MX6_DRAM_Stress_Test_Guide_vx.pdf document.
Can you send this to me?
Best Regards,
Yuuki
Hi Yuuki
please enter service request, I will send it to you.
Best regards
igor
Dear Igor-san,
Thank you for yoru support.
I made the following SR.
1-3694444541
Would you respond about this?
Best Regards,
Yuuki