About the display of logo in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the display of logo in uboot

768 Views
Joe_C
Contributor I

LOGO can be displayed on IMX8MQ SOC UBOOT, but when using the custom LOGO, the display is not normal, but the system's own LOGO can be displayed normally, the custom LOGO is also 8-bit BMP.How can I make the custom LOGO to display normally.

0 Kudos
Reply
2 Replies

665 Views
myy
Contributor II

Hi

how to init mipi dsi in uboot and display a logo

Tags (1)

762 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the link as below:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-ub...

though this is for imx6, but you can refer to it

0 Kudos
Reply