Hi community,
I found these is a new 3.10.31 kernel branch on the Freescale Git server.
I compare the 3.10.17 and 3.10.31 kernel patches about the gpu driver:
And I found there are some new patches in the 3.10.31 kernel.
Do you suggest to implement these new patches in the 3.10.17 kernel?
BR
Brian
已解决! 转到解答。
Hello Brian,
The one that you should use is the
Because this one is the tested release of the driver.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Brian,
The one that you should use is the
Because this one is the tested release of the driver.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------