Hello.
I want to check about i.MX6Q.
I want to enforce the "i.MX6 DDR Stress tester".
Please let me check the following.
①Could you the latest version of the "i.MX6 DDR Stress tester"?
I own the "DDR_Stress_Tester_V1.0.2".
②There is a specification of 1.2GHz (i.MX6Q) in "3.Select the ARM core speed" of User_Guide.
It is a "MCIMX6Q5EYM10AC" of the devices used.
This device is Frequency (1GHz).
Even in this case , ARM core speed will be set at 1.2GHz?
Regards,
-okamoto
已解决! 转到解答。
1.
Basically it is quite enough to use the "DDR_Stress_Tester_V1.0.2".
i.MX6 DDR Stress Test Tool V1.0.2
2.
"MCIMX6Q5EYM10AC" is not qualified for 1.2 MHz. This means, that customers
can try the device under 1.2 MHz, but we cannot guarantee proper operations with
parameters, provided in the Datasheet(s). Device lifetime also may be affected,
when using the device under non-specified conditions.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------