About behavior of SDIO controller for Errata No.13 of 1.MX21

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About behavior of SDIO controller for Errata No.13 of 1.MX21

跳至解决方案
998 次查看
yuuki
Senior Contributor II

I refer to errata No.13 of i.MX21.

MC9328MX21CE.pdf (rev6)

- No.13 (P.6)


The following contents are explained here.
"After sending the first block of data, the SDIO controller operation will stop if there is no BUSY signal responding from card be supported."

「the SDIO controller operation will stop」
Concretely, is it in what kind of situation?

Does SDCLK only stop?

Best Regards,

标记 (4)
0 项奖励
回复
1 解答
936 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Actually, the effect of this erratum can cause a write transfer error. However, most probably, in this case a transfer should just stall, and the MMC/SD host controller module would not report any valid transfer status. The reason is that the STATUS[CRC_WRITE_ERR] and STATUS[WR_CRC_ERROR_CODE] bits are valid only when a transfer is complete, i.e. when the STATUS[WRITE_OP_DONE] bit is set.


Hope this helps

Regards

在原帖中查看解决方案

0 项奖励
回复
3 回复数
936 次查看
YixingKong
Senior Contributor IV

Yuuki

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.

Thanks,
Yixing

0 项奖励
回复
936 次查看
yuuki
Senior Contributor II

Dear Bio_TICFSL-san, Yixing-san,

Thank you for your support.

The problem was solved.
I close this discussion.

Thank you.

0 项奖励
回复
937 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Actually, the effect of this erratum can cause a write transfer error. However, most probably, in this case a transfer should just stall, and the MMC/SD host controller module would not report any valid transfer status. The reason is that the STATUS[CRC_WRITE_ERR] and STATUS[WR_CRC_ERROR_CODE] bits are valid only when a transfer is complete, i.e. when the STATUS[WRITE_OP_DONE] bit is set.


Hope this helps

Regards

0 项奖励
回复