Dear All,
Hello. We want to add new camera sensor in i.MX6SL custom board.
I referred the "7.2 Adding Support for a New CMOS Camera Sensor" in i.MX 6 BSP Porting Guide, Rev. L3.14.28_1.0.0-ga, 04/2015.
[Q1]
i.MX6SL has no IPU.
And the L3.14.28_1.0.0 didn't support
I applied below patch. OV5642 works good on i.MX6SL EVK.
L3.14.28_1.0.0-Add-OV5642-subdev-driver.patch.zip
Re: About preview function in i.MX6SL.
Is it possible to apply Sect 7.2 to i.MX6SL to add new camera sensor?
(Or, is Sect 7.2 apply only for i.MX 6Q/D/DL/S?)
[Q2]
Do you have other information to add new camera sensor?
Best Regards,
Keita
Solved! Go to Solution.
The Section 7.2 of the BSP Porting Guide document you've mentioned just describes the general sequence of adding a new camera driver support into the package, so, it is applicable to the i.MX6SL package as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The Section 7.2 of the BSP Porting Guide document you've mentioned just describes the general sequence of adding a new camera driver support into the package, so, it is applicable to the i.MX6SL package as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------