Our customer is using the following development environment.
<Environment>
Baord: MX6Q-SABRE-SDB
Display: HDMI output
OS: AndroidKK4.4.2 FSL BSP
Package: AndroidKK4.4.2_Extended Feature Packages(android_kk4.4.2_1.0.0-ga_omxplayer_source)
Patchs: 0001-Fix-the-video-only-stream-can-t-play-issue.patch
html5_video_issue.patch
When a Video playback is repeated, the following error occurs.
And It seems that a Video application is finished forcibly(abnormal termination).
=====Error log=====
I/OMXPlayer( 2291): failed to open file: /data/system/audio_pass_through_pref.
W/linker ( 2291): lib_aac_dec_v2_arm12_elinux.so has text relocations. This is wasting memory and is a security risk. Please fix.
W/linker ( 2291): lib_aacplus_dec_v2_arm11_elinux.so has text relocations. This is wasting memory and is a security risk. Please fix.
===================
Are these errors related to abnormal termination?
May I have advice?
Best Regards,
Yuuki
Dear Sergio-san,
Thank you for your support.
I am sorry to delay.
Our customer uses the application of the partner.
Therefore I cannot provide the reproduction environment to you.
Would you teach the cause that you can suppose from contents of the error log?
Best Regards,
Yuuki
Dear Sergio-san,
We got a log by using this patch.
However, this log includes a confidential information.
Therefore we made a Service Request.
1-3768525447
Would you confirm this SR?
Best Regards,
Yuuki
Hello Yuuki,
Can you please share more information on how to apply the patches?:
1) baseline, commit hash id
2) whole patches with number 0001-*.patch, 0002-*.patch (i.e. 0001-Fix-* and html5_* which is the first?) . However, at this moment, I tried both sequence but failed to apply the two patches.
3) test files (media files)
4) the test steps.
5) run environment (i.e. boot from sd3 or mmc).