Dear Sir or Madam,
Hello.
Refer to "46.1 Introduction" in i.MX 6 Linux Reference Manual, Rev. L3.10.17_1.0.0-ga, 05/2014
========
If you want to use the DMA support for UART please also
enable the RTS/CTS for it. The DMA may be abnormal if you
do not enable the RTS/CTS.
========
I'd like to know the why FSL judged that RTS/CTS need.
(My customer will use SDMA with UART that do not enable the RTS/CTS.)
What problem did freescale face in the past?
Best Regards,
Keita
已解决! 转到解答。
UART interface is relatively slow, therefore special lines are required
for hardware ready acknowledgement, in order to avoid data FIFO overrun.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
UART interface is relatively slow, therefore special lines are required
for hardware ready acknowledgement, in order to avoid data FIFO overrun.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------