About Multi display in IMX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Multi display in IMX8QXP

1,660 Views
Zach4
Contributor I

Hi,

While connecting two displays to I.MX8.QXP Board using LVDS to HDMI one is showing Infotainment Screen and other one is showing a demo screen for Instrument cluster. I just want to make some changes to make the demo display to a working one. Could you help me to sort it out?.

Also an anybody tell me about audio configuration in the board also. Because while connecting the earphone to audio jack in the board and using the music player app inbuilt nothing is heard!

Regards,

Akhil

0 Kudos
Reply
5 Replies

1,629 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Akhil Raj,

To use two displays please refer to chapter 9.4.1 ''Booting with single LVDS-to-HDMI/MIPI-DSI-to-HDMI or dual LVDS-to-HDMI displays'' of Android_Quick_Start_Guide.pdf on page 61.

To configure your audio please refer to chapter 9.3 ''Flashing board images'' on Options for uuu_imx_android_flash tool:

To test the Sound Open Firmware audio output, execute the tool with -d sof

I will attach the file on this answer.

Best regards.

0 Kudos
Reply

1,585 Views
Zach4
Contributor I

Are there any ways we can modify or customize the demo cluster display in I.MX8 also could you please share the location of the source files of the cluster demo in the android build.

0 Kudos
Reply

1,568 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Akhil Raj,

To enable second display, you need go to init.rc, examlpe on MEK board:

# Enable second display

write /sys/class/drm/card0-HDMI-A-2/status on

write /sys/class/drm/card1-HDMI-A-2/status on

Best regards.

0 Kudos
Reply

1,642 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Akhil Raj,

Could you please share me your OS and version?

Best regards.

0 Kudos
Reply

1,639 Views
Zach4
Contributor I

Hi Jorge7u7

It's Android 12

0 Kudos
Reply