About MIPI interface of imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About MIPI interface of imx6

跳至解决方案
1,060 次查看
okamotosatoshi
Contributor IV

Hi There,

I want to check for IMX6.
Unused MIPI recommends "Leave unconnected".

Hardware Development Guide for i.MX 6DualPlus/6QuadPlus, 6Dual/6Quad and i.MX 6Solo/6DualLite Applications Processors
2.8 Unused analog interfaces

Is this due to shutting down the PHY?

We are considering whether termination is necessary when the camera is not in use.
Is it possible to terminate (for internal IMX6) MIPI CSI?
Do I have to terminate externally?

Best regards
- satoshi

标签 (4)
0 项奖励
回复
1 解答
906 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please just follow recommendations of the Hardware Development Guide :

no need for termination of the mentioned signals.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
907 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please just follow recommendations of the Hardware Development Guide :

no need for termination of the mentioned signals.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复
906 次查看
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for your advice.
We will consider countermeasures against noise when not in use.

Very Thanks.

Best regards
- satoshi

0 项奖励
回复