About Hold Delay of QuadSPI configuration parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Hold Delay of QuadSPI configuration parameters

ソリューションへジャンプ
858件の閲覧回数
goto11
Contributor III

Hello,

Isn't the Hold Delay of 6.6.6.3 (QuadSPI configuration parameters) in the i.MX 7Dual Applications Processor Reference Manual the TDH setting of 10.2.14.3 (QuadSPIx_FLSHCR)?

If not TDH, where can I find a description of Hold Delay?

best regards
Goto

ラベル(1)
0 件の賞賛
1 解決策
830件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

    Recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)]  corresponds
QuadSPI configuration boot parameter Hold Delay. 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
853件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   Hold Delay for quarter cycle is used for DDR mode.

Regards,
Yuri.

0 件の賞賛
848件の閲覧回数
goto11
Contributor III

Hello,

 

Does Hold Delay mean that the quarter cycle is used in DDR mode, which means that it is set to the TDH setting "01" of 10.2.14.3 (QuadSPIx_FLSHCR)?

If so, should it be set to "01" in DDR mode (DDR_EN = 1)?

Regards,
Goto

0 件の賞賛
831件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

    Recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)]  corresponds
QuadSPI configuration boot parameter Hold Delay. 

Regards,
Yuri.

0 件の賞賛