@goto11
Hello,
Recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)] corresponds
QuadSPI configuration boot parameter Hold Delay.
Regards,
Yuri.
Hello,
Does Hold Delay mean that the quarter cycle is used in DDR mode, which means that it is set to the TDH setting "01" of 10.2.14.3 (QuadSPIx_FLSHCR)?
If so, should it be set to "01" in DDR mode (DDR_EN = 1)?
Regards,
Goto
@goto11
Hello,
Recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)] corresponds
QuadSPI configuration boot parameter Hold Delay.
Regards,
Yuri.