About the parameters of Table 6-50 of i.MX 7 Dual Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the parameters of Table 6-50 of i.MX 7 Dual Reference Manual

Jump to solution
473 Views
goto11
Contributor III

Hello,

I have two questions.

No1
There is a Hold Delay in the Table.
Does the combination in Description enable the quarter cycle Delay in DDR mode?

No2
QuadSPIx_FLSHCR on 10.2.14.3 has a TDH setting.
Are this setting and Hold Delay in Table 6-50 the same setting?

best regards
Goto

Labels (1)
0 Kudos
1 Solution
467 Views
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   Yes, recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)]  corresponds
QuadSPI configuration boot parameter Hold Delay.

 

Regards,
Yuri.

View solution in original post

0 Kudos
1 Reply
468 Views
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,

   Yes, recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)]  corresponds
QuadSPI configuration boot parameter Hold Delay.

 

Regards,
Yuri.

0 Kudos