About ERR004364 uSDHC: Limitations on uSDHC3 and uSDHC4 clock-gating in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ERR004364 uSDHC: Limitations on uSDHC3 and uSDHC4 clock-gating in i.MX6DQ.

ソリューションへジャンプ
578件の閲覧回数
keitanagashima
Senior Contributor I


Der All,

Refer to ERR004364 in IMX6DQCE(Rev.6).

The impact is RAWNAND and APBHDMA clocks might be gated unintentionally.

And, "Functionality or mode of operation in which the erratum may manifest itself is not used".

Now, my customer is using only uSDHC3, but not using GPMI.

Is it possible to ignore this errata on customer's system?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
501件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the ERR004364 erratum can be ignored if the NAND GPMI controller is not in use.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
502件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the ERR004364 erratum can be ignored if the NAND GPMI controller is not in use.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信