AUDMUX port3 connect port4 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AUDMUX port3 connect port4 issue

ソリューションへジャンプ
744件の閲覧回数
felixhsu
Contributor III

Hi all

pastedImage_1.png

In the IMX6DQRM document this section explanation port to port relationship,

the red color box meaning is port 3 can connect to port 4, it is correct or not ?

Please help me clarify this issue, thanks.

ラベル(2)
0 件の賞賛
1 解決策
525件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

description is correct also please refer to RM in

sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :

TFSEL=3, TCSEL=3

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
525件の閲覧回数
felixhsu
Contributor III

Hi igorpadykov

Thank your reply.

I have another question for AUDMUX.

If use two I2S output path, may I can use different BCLK for each output or not?

Such as 1.536MHz and 3.072MHZ.

0 件の賞賛
525件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes each audmux port can have different BCLK.

0 件の賞賛
526件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

description is correct also please refer to RM in

sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :

TFSEL=3, TCSEL=3

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛