AUDMUX port3 connect port4 issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUDMUX port3 connect port4 issue

Jump to solution
857 Views
felixhsu
Contributor III

Hi all

pastedImage_1.png

In the IMX6DQRM document this section explanation port to port relationship,

the red color box meaning is port 3 can connect to port 4, it is correct or not ?

Please help me clarify this issue, thanks.

Labels (2)
0 Kudos
Reply
1 Solution
638 Views
igorpadykov
NXP Employee
NXP Employee

Hi Felix

description is correct also please refer to RM in

sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :

TFSEL=3, TCSEL=3

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
638 Views
felixhsu
Contributor III

Hi igorpadykov

Thank your reply.

I have another question for AUDMUX.

If use two I2S output path, may I can use different BCLK for each output or not?

Such as 1.536MHz and 3.072MHZ.

0 Kudos
Reply
638 Views
igorpadykov
NXP Employee
NXP Employee

yes each audmux port can have different BCLK.

0 Kudos
Reply
639 Views
igorpadykov
NXP Employee
NXP Employee

Hi Felix

description is correct also please refer to RM in

sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :

TFSEL=3, TCSEL=3

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply