Hi all
In the IMX6DQRM document this section explanation port to port relationship,
the red color box meaning is port 3 can connect to port 4, it is correct or not ?
Please help me clarify this issue, thanks.
Solved! Go to Solution.
Hi Felix
description is correct also please refer to RM in
sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :
TFSEL=3, TCSEL=3
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
Thank your reply.
I have another question for AUDMUX.
If use two I2S output path, may I can use different BCLK for each output or not?
Such as 1.536MHz and 3.072MHZ.
yes each audmux port can have different BCLK.
Hi Felix
description is correct also please refer to RM in
sect.16.6.5 Port Timing Control Register 3 (AUDMUX_PTCR3) :
TFSEL=3, TCSEL=3
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------