imx6接收到914输出的数据后,得到的图像几乎是绿色。硬件VS HS PCLK都是正常的,8根数据线也正常。
下面是914对接imx6的原理图
913用的低8bit,914选着10bit模式,其中914只有D0-D7有数据过来,imx6 D10-D17有数据过来。
我看官方这块是D12-D19接的是ov5642,所以不知道是不是914要接到imx6的高8位图像才会正常输出?
附上采集到的图像:
Hello Yabin,
使用I.MX6Q CSI并行接口时,如果是YUV或者BT.656格式 8bit模式,确实是需要接在D12~D19上的。
Have a nice day!
TIC weidong sun
Hi Wigros,
这块为什么要接到D12~D19上呢,手册中也没提到,这是为什么呢?您之前是做过类似的试验吗
Hi Wigros,
官方接的ov5642数据确实是D12~D19,这块手册中并没有提及到是为什么,您知道这是为什么吗?
还是您之前做过类似的试验呢?