Dear all,
We have heard that 90 degrees rotation for Full-HD using IRT (ImageRotator) cannot be performed in i.MX6.
* It is described by this URL, for example. --> i.MX6 IPU and rotating a frame buffer
We expect that it is possible in QuadPlus.
Is it possible in QualPlus?
Best Regards,
George
已解决! 转到解答。
Hi George
IPU module is the same in QuadPlus, so capabilities the same.
QuadPlus improved bus architecture and add/(fixed errata) some modules
for improving ddr performance
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi George
IPU module is the same in QuadPlus, so capabilities the same.
QuadPlus improved bus architecture and add/(fixed errata) some modules
for improving ddr performance
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi George,
I tried the patch from Marco Antonio Segalla Cassol (Re: i.MX6 IPU and rotating a frame buffer) and I can rotate the FullHD HDMI output.
Though I don't know if there are any other limitations.
Best Regards
Frieder
Dear Frieder,
You are wonderful !!
It had not tried, though I was also reading the thread.
However, I will try it like you.
Please let me know Kernel Command Line Option which you used.
Is the following correct?
"console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,ROTATE=4"
Best Regards,
George
Hi George,
I used this for the video parameter:
video=mxcfb0:dev=hdmi,1920x1080M@60,rotate=4,if=RGB24
But it seems like it doesn't work on all screens. I have a HDMI screen that says "input not supported" if rotate is between 4 and 7.
On a different screen all rotation options seem to work.
I haven't tested LCD and LVDS screens so far.
Best Regards
Frieder