Can not see pcie on i.MX8QXP internal PLL with Android Automotive 12.0.0_2.1.0 (Linux 5.15.32 BSP)
mek_8q:/ # zcat /proc/config.gz | grep -i imx_pci
CONFIG_PHY_FSL_IMX_PCIE=y
mek_8q:/ # zcat /proc/config.gz | grep -i pci_imx
CONFIG_PCI_IMX6=y
CONFIG_PCI_IMX6_HOST=y
mek_8q:/ # dmesg | grep -i pci
[ 0.000000] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init androidboot.hardware=nxp firmware_class.pe
[ 0.314189] PCI: CLS 0 bytes, default 64
[ 2.834329] tcpci: probe of 1-0050 failed with error -1
mek_8q:/ # lspci
mek_8q:/ #
The HW should be ok since we can see it in uboot(Please ignore gpio error, for quick test we did'nt set it yet.)
=> pci
pca953x gpio@1a: Error reading output register
imx_pcie pcie@0x5f010000: -16 unable to get clkreq.
imx_pcie pcie@0x5f010000: -2 unable to get disable-gpio.
pca953x gpio@1a: Error reading output register
imx_pcie pcie@0x5f010000: 3 unable to get power-on-gpio.
imx_pcie pcie@0x5f010000: -16 unable to get power-on-gpio.
PCI: pcie phy link never came up
Also we can see it on linux with this dts config
&pcieb{
ext_osc = <0>;
};
解決済! 解決策の投稿を見る。