[8MPlus][EVK][ASRC] Detect underrun at 176.4kHz~384kHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[8MPlus][EVK][ASRC] Detect underrun at 176.4kHz~384kHz

1,079件の閲覧回数
masahiro_inamur
Contributor III

Dear  @shigenobukatagi  san,
cc @wataken  san

We are investigating ASRC on 8MPlus EVK with L5.15.5_1.0.0_MX8MP kernel source.
During this investigation, we detected some "underrun" at 176.4kHz~384kHz@16bit by using the following command.

Could you provide some countermeasure for it?

■FW
L5.15.5_1.0.0_MX8MP
https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-... 

■Command (Sound card)

card 4: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 [HiFi wm8960-hifi-0]


Best Regards,
Inamura

0 件の賞賛
返信
5 返答(返信)

1,070件の閲覧回数
shigenobukatagi
NXP Employee
NXP Employee

@atsushihonda san,

Can you please look at the issue?

Best Regards,
Shigenobu

0 件の賞賛
返信

1,056件の閲覧回数
atsushihonda
NXP Employee
NXP Employee

Hi @masahiro_inamur san, @wataken san

It seems that the command is not seen. Could you please send the command that shows underrun?

 

@shigenobukatagi 

Best regards,
Atsushi Honda

0 件の賞賛
返信

1,050件の閲覧回数
masahiro_inamur
Contributor III

Hi, @atsushihonda san,

Sorry for confusing you.

We use the following aplay command.

 

root@imx8mpevk:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: btscoaudio [bt-sco-audio], device 0: 30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0 [30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 2: imxaudioxcvr [imx-audio-xcvr], device 0: XCVR PCM snd-soc-dummy-dai-0 [XCVR PCM snd-soc-dummy-dai-0]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 3: audiohdmi [audio-hdmi], device 0: i.MX HDMI i2s-hifi-0 [i.MX HDMI i2s-hifi-0]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 4: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 [HiFi wm8960-hifi-0]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 4: wm8960audio [wm8960-audio], device 1: HiFi-ASRC-FE (*) []
  Subdevices: 1/1
  Subdevice #0: subdevice #0
aplay -D hw:4,1 xxx.wav

 


Best Regards,
Inamura

0 件の賞賛
返信

1,034件の閲覧回数
atsushihonda
NXP Employee
NXP Employee

Hi @masahiro_inamur san,

Thanks for your information.

We just noticed that it is better to communicate this in your private audio community site, instead of here.
Could you please open another ticket in your private audio community site?

 

Best regards,
Atsushi Honda

0 件の賞賛
返信

1,022件の閲覧回数
masahiro_inamur
Contributor III

Hi, @atsushihonda san,

Noted on this.
I will open another ticket in audio community site.

Best regards,
Inamura

0 件の賞賛
返信