iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

cancel
Showing results for 
Search instead for 
Did you mean: 

iMX8M NANO with SD card can't install Android 10 but can install Android 11 by uuu.exe

116 Views
steveyang2
Contributor I

Try to use uuu.exe build Android 10 in windows 10 but meet error.

Please help me confirm the root cause.

 

Android Q10.0.0_2.6.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Error message : 1/1 [HID(W):LIBUSB_ERROR_TIMOUT ] SDPS: boot -f u-boot-imx8mn-evk-uuu.imx.link

 

Android 11.0.0_2.4.0

Command :  .\uuu_imx_android_flash.bat -f imx8mn -c -e -t sd

Build successfully

0 Kudos
1 Reply

105 Views
Harvey021
NXP Employee
NXP Employee

Hi @steveyang2 

I run the same command with prebuilt images - android-10.0.0_2.6.0_image_8mnevk. and it works without such error.

Please check if all necessary software images that you are going to build for these command are included and without broken ones.

 

Best regards

Harvey

 

0 Kudos