8MNANOD4-EVK can't initialize bluetooth but WiFi is working well

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8MNANOD4-EVK can't initialize bluetooth but WiFi is working well

Jump to solution
773 Views
Luke-Hsieh
Contributor III

After the brcmfmac driver was builtin, the WiFi was able to connect to my WiFi AP and access to the internet resources.

 

However, I can't bring up the "hci0" interface successfully even the "BD Address: 00:00:00:00:00:00" is wrong.

 

 

root@imx8mnddr4evk:~# uname -a
Linux imx8mnddr4evk 5.15.32-lts-next+gfa6c3168595c #1 SMP PREEMPT Tue Jun 7 02:34:46 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux

 

root@imx8mnddr4evk:~# dmesg|grep brcm
[ 5.474354] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6
[ 5.621392] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac43455-sdio for chip BCM4345/6
[ 5.644172] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4345/6 wl0: Mar 3 2019 19:47:25 version 7.45.184 (r712131 CY) FWID 01-b363c0a0

 

root@imx8mnddr4evk:~# hciattach /dev/ttymxc0 any 115200 flow
Setting TTY to N_HCI line discipline
Device setup complete
root@imx8mnddr4evk:~# [ 18.110681] Bluetooth: hci0: command 0x1003 tx timeout
[ 20.126664] Bluetooth: hci0: command 0x1001 tx timeout
[ 22.142681] Bluetooth: hci0: command 0x1009 tx timeout

 

root@imx8mnddr4evk:~# hciconfig
hci0: Type: Primary Bus: UART
BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0
DOWN
RX bytes:0 acl:0 sco:0 events:0 errors:0
TX bytes:12 acl:0 sco:0 commands:3 errors:0

 

Labels (1)
0 Kudos
1 Solution
720 Views
Luke-Hsieh
Contributor III

Hi Jimmy,

 

Thanks for the INFO.

I'll try it on L5.4.24_2.1.0 BSP release.

 

 

View solution in original post

0 Kudos
4 Replies
743 Views
jimmychan
NXP TechSupport
NXP TechSupport

Could you tell me which wifi/bt chip are you using on the evk board?

0 Kudos
739 Views
Luke-Hsieh
Contributor III

Hi Jimmy,

 

The printing of U6 component on my EV board is not clear, but I think it should be a Cypress CYW43455 chip according to the INFO in 3.10 of 8MNANOD4-EVK hardware user's guide.

Also, the wlan0 interface was working after the Broadcom's driver was inserted, so I think the INFO in the user is correct.

 


3.10. Wi-Fi/Bluetooth (U6)
The EVK board has a Wi-Fi/Bluetooth module LBEE5HY1MW on the 8MNANOD4-CPU board. The module is Cypress CYW43455 based, contains SDIO3.0, UART, PCM interface, and can support 802.11a/b/g/n/ac, BT5.0.

0 Kudos
729 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the L5.15.32 BSP release notes, CYW43455 is not in the support list.

In the L5.4.24_2.1.0, CYW43455 is in the support list. You may try to use the version L5.4.24_2.1.0 BSP.

 

Here is the Linux BSP web page.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

 

0 Kudos
721 Views
Luke-Hsieh
Contributor III

Hi Jimmy,

 

Thanks for the INFO.

I'll try it on L5.4.24_2.1.0 BSP release.

 

 

0 Kudos