8MMINILPD4-EVK baseboard design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8MMINILPD4-EVK baseboard design

751件の閲覧回数
ashish_m
Contributor I

Hi

we are designing customized board w.r.t 8MMINILPD4-EVK board

We have following requirements:

  • 13.8V supply to power carrier board from J101 connector.
  • USB1 to connect external hard disk using type c connector.
  • USB2 interface with FT232R (USB UART IC )

Planning to remove type c connector (J302) and connect USB2 DP DN connector to FT232.

 For above requirements we have following queries

  • changes needed to be done in hardware
  • configuration to be done in IC U302,U303,U305,U306

 

0 件の賞賛
返信
0 返答(返信)