Use IMX8M to drive 88W8997 with wlan: version=SD8997---16.92.21. p84.4-MM5X16391. p3-GPL - (FP92), and use the following instructions to test the 5GRF parameters
Echo "rf_test_mode=1">/proc/mwlan/adapter0/config
Echo "rx_antenna=3">/proc/mwlan/adapter0/config
Echo "tx_antenna=3">/proc/mwlan/adapter0/config
Echo "band=1">>/proc/mwlan/adapter0/config
Echo "tx_power=10 2 2">/proc/mwlan/adapter0/config
Echo "tx_continuous=1 1 0xAAA 0 3 7">/proc/mwlan/adapter0/config
The power configuration is 10dbm, but the test result is -7.3dbm, but the 2.4G test is normal. Do you need to configure other parameters????