hello,
We're using camera 5MP ov5640 for imx6Dual Lite. But now we're going to change to use higher camera (8MP).
Could you please give me a suggestion about the best of camera that we should use for imx6 among below list.
Part number | Mfr | Compatibility (Y/N) |
OV8858 | Omnivision |
|
OV8865 | Omnivision |
|
OV8856 | Omnivision |
|
OS08A10 | Omnivision |
|
VB6955CM | Stmicro |
|
AR0833 | Onsemi |
|
IMX179 | Sony |
|
IM219PQ | Sony |
|
which one was already supported driver and BSP? In the linux kernel for imx6 version 4.1.15, I just see driver for ov5640, ov5642, ov5647 with 5MP.
Thanks in advance.
Dong
Details data reference you can refer to the i.MX6DQ Reference Manual. And the follow thread maybe do some help for you.https://community.nxp.com/message/941201?commentID=941201#comment-941201
Hi Dong,
As you said obove, in our default BSP only driver for ov5640, ov5642, ov5647 with 5MP are supported. About the 8MP
you need to do porting yourself.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rita,
Thanks so much for your respond.
Dong