8 megapixel , which camera should we use for imx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8 megapixel , which camera should we use for imx6?

1,614 Views
dongpv
Contributor III

hello,

We're using camera 5MP ov5640 for imx6Dual Lite. But now we're going to change to use higher camera (8MP).

Could you please give me a suggestion about the best of camera that we should use for imx6 among below list.

Part number

Mfr

Compatibility (Y/N)

OV8858

Omnivision

 

OV8865

Omnivision

 

OV8856

Omnivision

 

OS08A10

Omnivision

 

VB6955CM   

Stmicro

 

AR0833

Onsemi

 

IMX179

Sony

 

IM219PQ

Sony

 

which one was already supported driver and BSP? In the linux kernel for imx6 version 4.1.15, I just see driver for ov5640, ov5642, ov5647 with 5MP.

Thanks in advance.

Dong

3 Replies

983 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Details data reference you can refer to the i.MX6DQ Reference Manual. And the follow thread maybe do some help for you.https://community.nxp.com/message/941201?commentID=941201#comment-941201 

983 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Dong,

As you said obove, in our default BSP only driver for ov5640, ov5642, ov5647 with 5MP are supported. About the 8MP

you need to do porting yourself.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

983 Views
dongpv
Contributor III

Hi Rita,

Thanks so much for your respond.

Dong

0 Kudos