What are 15 W wireless charging single-coil transmitter and receiver development board part number?
I'm going to buy them. Please help to provide it.
Thanks a lot.
Hi,
For the transmitter, I would recommend the 15-watt single-coil wireless charging transmitter reference platform, WCT-15W1COILTX, which is based on the NXP MWCT1012CFM transmit controller IC: https://www.nxp.com/support/developer-resources/nxp-designs/wct-15w1coiltx-15-w-single-coil-wireless...
As per the Receiver, I recommend the WCR1516 wireless charger receiver to support up to 15W. There are 2 different reference designs for this receiver:
Have a great day,
Jose
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Jose:
Thanks for your support.
I Check to NXP web prompted "WCT-15W1COILTX is not recommended for new designs".
Please help to confirm it. Thanks
Hi,
You are correct, sorry about that.
Then currently, for 15W solution, we only have the WCT-15WTXAUTO, which is a 15W multi-coil transmitter reference platform is designed for automotive wireless charging applications based on the NXP MWCT1013AVLH transmit controller IC.
Currently there is no solution board for 15W single-coil transmitter.