15 W wireless charging single-coil transmitter and receiver development board part number?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

15 W wireless charging single-coil transmitter and receiver development board part number?

962 Views
join_ren
Contributor III

What are 15 W wireless charging single-coil transmitter and  receiver development board part number?

I'm going to buy them.  Please help to provide it. 

Thanks a lot.

Labels (1)
0 Kudos
3 Replies

810 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

For the transmitter, I would recommend the 15-watt single-coil wireless charging transmitter reference platform, WCT-15W1COILTX, which is based on the NXP MWCT1012CFM transmit controller IC: https://www.nxp.com/support/developer-resources/nxp-designs/wct-15w1coiltx-15-w-single-coil-wireless...

 

As per the Receiver, I recommend the WCR1516 wireless charger receiver to support up to 15W. There are 2 different reference designs for this receiver:

 

  1. WPR1500-LDO. Supports 5V/3A output following the WPC “Qi” specification. With only rectifier and LDO MOSFET outside WPR1516 for system thermal design. Most optimized BOM cost: https://www.nxp.com/support/developer-resources/nxp-designs/wpr1500-ldo-15-w-wireless-charging-recei...

 

  1. WPR1500-BUCK. Output with Buck architecture which approves 5V/3A following WPC “Qi” specification, and with capability to support other output voltage and current for various battery configuration: https://www.nxp.com/support/developer-resources/nxp-designs/wpr1500-buck-15-w-wireless-charging-rece...

Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

811 Views
join_ren
Contributor III

WCT-15W1COILTX.JPG

Hi Jose:

Thanks for your support.

I Check to NXP web prompted "WCT-15W1COILTX is not recommended for new designs".

Please help to confirm it. Thanks

 

0 Kudos

811 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

You are correct, sorry about that.

 

Then currently, for 15W solution, we only have the WCT-15WTXAUTO, which is a 15W multi-coil transmitter reference platform is designed for automotive wireless charging applications based on the NXP MWCT1013AVLH transmit controller IC.

https://www.nxp.com/support/developer-resources/nxp-designs/wct-15wtxauto-multi-coil-wireless-chargi...

 

Currently there is no solution board for 15W single-coil transmitter.

0 Kudos