执行出现错误 ./mxc_vpu_test.out -E "-w 176 -h 144 -f 0 -o enc.m4v"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

执行出现错误 ./mxc_vpu_test.out -E "-w 176 -h 144 -f 0 -o enc.m4v"

977 Views
画梁佳
Contributor I
[INFO]Product Info: i.MX6Q/D/S
[INFO]VPU firmware version: 2.3.10_r40778
[INFO]VPU library version: 5.4.16
[INFO]Format: STD_MPEG4
[INFO]MPEG4 class: MPEG4
[INFO]Output file "enc.m4v" opened.
[INFO]Product Info: i.MX6Q/D/S
[INFO]VPU firmware version: 2.3.10_r40778
[INFO]VPU library version: 5.4.16
[INFO]Capture/Encode fps will be 30
[INFO]chromaInterleave 1, mapType 0, linear2TiledEnable 0

ov3640_write_reg:write reg error:reg=3012,val=80

[INFO]sensor chip is ov5640_camera

Not support the resolution in camera

麻烦大师帮我看看,应该怎么解决。

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

804 Views
joanxie
NXP TechSupport
NXP TechSupport

for your new camera, did you build in the bsp? if not, pls build this camera in the bsp first

0 Kudos
Reply

804 Views
joanxie
NXP TechSupport
NXP TechSupport

did you use ov3640?

pls try to use two commands before use unit test

"

modprobe mxc_v4l_capture

modprobe ov3640_camera

"

0 Kudos
Reply

804 Views
画梁佳
Contributor I

你好,我使用的是usb摄像头。

0 Kudos
Reply