我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

755件の閲覧回数
chengzhiyan
Contributor I

我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢

0 件の賞賛
返信
3 返答(返信)

607件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chengzhi yan,

Which board are you using , is it the board i.MX51 Evaluation Kit you buy from NXP ? If yes, you can use the mfgtool in our website to write the images to the SD on your board. The Root File System for the Ubuntu Demo image you can download from our website. The link is :

i.MX51 Evaluation Kit|NXP . You can see it under the

Root File System for the Ubuntu Demo Image. ER 2010.11 for i.MX51. Engineering Release (REV ER2010.11)

  Root File System for the Ubuntu Demo Image. ER 2010.11 for i.MX51. Engineering Release.

Hope this can help you.

Have a nice day.

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

607件の閲覧回数
chengzhiyan
Contributor I

It is ok,thank you!

0 件の賞賛
返信

607件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chengzhi yan,

:smileyhappy:I am very glad it can help you. If this post answers your question, please click the Correct Answer button. Thank you!

Have a nice day

Best Regards

Dan

0 件の賞賛
返信