我的imax51开发板,自带的sd卡丢失了。如何恢复自带的sd卡内的Ubuntu系统?谢谢
Hi chengzhi yan,
Which board are you using , is it the board i.MX51 Evaluation Kit you buy from NXP ? If yes, you can use the mfgtool in our website to write the images to the SD on your board. The Root File System for the Ubuntu Demo image you can download from our website. The link is :
i.MX51 Evaluation Kit|NXP . You can see it under the
Root File System for the Ubuntu Demo Image. ER 2010.11 for i.MX51. Engineering Release.
Hope this can help you.
Have a nice day.
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------