我已经在zlib官网下了最新的 然后默认的配置安装了 但是在./ltib时候 提示我没有安装zlib 请问是路劲问题吗 我的ubuntu是12.04 这个要如何解决呢 看了社区的一些老帖子 是ubuntu9.04上解决这个问题的 但是那个帖子说 方法不适用其他版本ubuntu
解決済! 解決策の投稿を見る。
Hi Nan,
Is this issue still?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nan,
Is this issue still?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Dan
i have solved this problem and compiled successful
thanks
Hi Nan,
Are you using the 32bit Ubuntu 12.04 or 64bit Ubuntu?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
32bit
Hi nan,
If you are using the 32bit ubuntu, and you meet the Zlib -------Uninstall when you use the LTIB to build the BSP.
Here you have to make sure that the lib.So point to the correct on in system. You can see it in the ltib/bin/Ltibutils.Pm. Here you have already solved the questions by apply the patch.
About the failed downloading packages, can you tell me which BSP and board are you using?
Best Regards
Dan
hello Dan
sorry ,my english not well. this my first use imx6q .my board is imx6q SABRE, what means " which BSP i use", i download package "L3.0.35_4.1.0_130816_source.tar.gz" then i begain install the source and "./ltip".
Hi Nan,
It's OK, you can speak Chinese here. The L3.0.35_4.1.0_130816_source.tar.gz is your BSP:smileyhappy:. When you install the source code and LTIB, you can refer to our user guide and the document I attached for you.
Any questions contact me easily.
Have a great day,
Dan
Hi Dan
我按照你的文档做了一遍。但是最后一步出错,有朋友注释掉源码解决了这个问题 ,但我不知道这样做是不是对的。所以请看下我的日志,这个问题比较普遍,麻烦找下问题。下面是日志
Build path taken because: directory build, no prebuilt rpm,
Cowardly refusing to clobber existing directory:
/opt/freescale/ltib/usr/src/rpm/BUILD/mtd-utils
Remove this by hand if you really want to rebuild this package from scratch
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
Started: Thu Mar 3 16:59:16 2016
Ended: Thu Mar 3 16:59:16 2016
Elapsed: 0 seconds
These packages failed to build:
mtd-utils
Build Failed
谢谢
Hi Dan
i will refer to your attached document.
thank you
通过官网的补丁可以解决这个问题 但是我发现在安装LTIB时有很多文件无法下载下来 似乎有网络的问题 还有下载地址的问题 非常多的文件无法下载 如果要手动一个一个下载下来的话 感觉会疯的。。。有什么方法解决吗
Hi Nan,
Which BSP and board are you using?
Best Regards
Dan
board is imx6q and BSP is L3.0.35_4.1.0_130816_source
thank you
Hi Nan,
I have written a document about download and build this version BSP. You can refer to .
My environment is as follow
PC: VMware Player Ubuntu 12.04 64bit LTS
Linux BSP Source Code: L3.0.35_4.1.0_ER_SOURCE_BSP
Board: i.MX6DL-SDP
Hope this can help you.
Any questions contact me easily.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello Dan
i will learning from your attached document.then after this i have questions ,i wil communicate with you.
thank you for your help