关于Android 7.1.1 Nougat (N7.1.1_1.0.0)se的bsp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于Android 7.1.1 Nougat (N7.1.1_1.0.0)se的bsp

1,326 Views
jiangshao
Contributor V

各位尊敬的FAE

 

我有一块客户的开发板MX6-SabreSD,imx6q+2G RAM,从nxp官网下载Nougat源码编译后,烧写,修改uboot参数,改为HDMI输出。可以看到Android的logo,但是串口0输出错误信息后启动中止。具体请看附件。

有谁遇到过类似问题吗?

以前同样的硬件在android5.1和Android6.0.1上没有类似问题。

Original Attachment has been moved to: android711.log.zip

Labels (5)
0 Kudos
Reply
1 Reply

1,110 Views
weidong_sun
NXP TechSupport
NXP TechSupport

你好,这个问题,请你这样做一下,试试:

(1)从我们网站上下载demo image,android7.1.1的。然后烧写进SD卡,启动一下。

(2)如果DEMO image是正常启动的,说明硬件OK。你再编译源码。

(3)要注意的是,源码里默认是支持从板上eMMC启动的。所以,你要烧写进eMMC才行。


Have a great day,
TIC   weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply