关于用两块USB2514扩展USB port的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于用两块USB2514扩展USB port的问题

Jump to solution
25,270 Views
jiangshao
Contributor V

各位FAE

我有一块客户定制的imx6q sabresd的开发板,OS为安卓4.2.2。

如附件的示意图所示,

第一块2514的port1用来连接第二块2514,

第一块2514的port2用来连接3G/4G模块,

其余的USB port开放给用户。

但是现在有个奇怪的问题,那就是第二块2514的4个USB port虽然可以正常使用mouse等设备,

却无法识别U盘,3G/4G模块等设备。

在使用两块2514来扩展USB port时有什么需要注意的问题吗?

Labels (4)
0 Kudos
Reply
1 Solution
24,385 Views
jiangshao
Contributor V

从dmesg的输出看也是bus power不足。后来厂家确认是焊接问题。

View solution in original post

0 Kudos
Reply
3 Replies
24,385 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

你这里是不是电流不够

0 Kudos
Reply
24,386 Views
jiangshao
Contributor V

从dmesg的输出看也是bus power不足。后来厂家确认是焊接问题。

0 Kudos
Reply
24,385 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK. Good news. 问题解决了就好

0 Kudos
Reply