Translated by Google:
Use KSZ9031 IC, Ethernet can not use the 1000M Lan
We are using KSZ9031 scenario, if set to 10M / 100M no problem, but if set to 1000M, you can not connect.
Router supports the 1000M.
-------------------------------------------------
Hi Guo
suggest to check Table 62. RGMII Signal Switching Specifications IMX6DQCEC
and configure KSZ9031 registers if necessary, like
MMD Address 2h Register 5h - RGMII RX Data Pad Skew
MMD Address 2h Register 6h - RGMII TX Data Pad Skew
MMD Address 2h Register 8h - RGMII Clock Pad Skew
Note, for i.MX6 ENET there is no control on-chip to adjust the delay between
these signals. A delay would need to be implemented at the board level.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------