iMX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0 GA Release

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0 GA Release

iMX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0 GA Release


The i.MX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0 GA release is now available on www.freescale.com

·         Files available

         

Name

Description

L3.10.53_1.1.0_LINUX_DOCS

i.MX 6 D/Q/DL/S/SL Linux   3.10.53_1.1.0 GA BSP documentation.

L3.10.53_1.1.0_iMX6QDLS_Bundle

i.MX 6 D/Q/DL/S  Linux   3.10.53_1.1.0 GA BSP Binary Demo Files

L3.10.53_1.1.0_iMX6SL_Bundle

i.MX 6 SL  Linux   3.10.53_1.1.0 GA BSP Binary Demo Files

L3.10.53_1.1.0_AACP_CODECS

AAC Plus Codec for the i.MX 6 D/Q/DL/S/SL Linux 3.10.53_1.1.0   GA BSP y

IMX_6_MFG_L3.10.53_1.1.0_TOOL

Manufacturing Tool and Documentation for Linux   3.10.53_1.1.0 GA BSP y

·         Target HW boards

o   i.MX6DL  SABRE SD board

o   i.MX6Q  SABRE SD board

o   i.MX6DQ SABRE AI board

o   i.MX6DL SABRE AI board

o   i.MX6SL EVK board

New Features

·                             Please refer to formal Release Note document for all details.

Known issues

For known issues and limitations please consult the release notes located in the BSP documentation package.

标签 (2)
标记 (1)
无评分
版本历史
最后更新:
‎02-03-2015 03:48 PM
更新人: