Hello!
Here's some CODE!!!
#include <iostream>
#include <stdio.h>
#include <assert.h>
#include <string.h>
#include <fcntl.h>
#include <malloc.h>
#include <math.h>
#include <stdlib.h>
//#define EGL_USE_GLES2
#include <GLES2/gl2.h>
#include <EGL/egl.h>
#include <GLES2/gl2ext.h>
#include <EGL/eglext.h>
#include <termios.h>
#include <unistd.h>
#include <fcntl.h>
#ifdef EGL_USE_X11
#include <X11/X.h>
#include <X11/Xlib.h>
#endif
EGLDisplay egldisplay;
EGLConfig eglconfig;
EGLSurface eglsurface;
EGLContext eglcontext;
EGLNativeWindowType eglNativeWindow;
EGLNativeDisplayType eglNativeDisplayType;
EGLNativeDisplayType fsl_getNativeDisplay()
{
EGLNativeDisplayType eglNativeDisplayType = NULL;
#if (defined EGL_USE_X11)
eglNativeDisplayType = XOpenDisplay(NULL);
assert(eglNativeDisplayType != NULL);
#elif (defined EGL_API_FB)
eglNativeDisplayType = fbGetDisplayByIndex(0); //Pass the argument as required to show the framebuffer
#else
display = EGL_DEFAULT_DISPLAY;
#endif
return eglNativeDisplayType;
}
EGLNativeWindowType fsl_createwindow(EGLDisplay egldisplay, EGLNativeDisplayType eglNativeDisplayType)
{
EGLNativeWindowType native_window = (EGLNativeWindowType)0;
#if (defined EGL_USE_X11)
Window window, rootwindow;
int screen = DefaultScreen(eglNativeDisplayType);
rootwindow = RootWindow(eglNativeDisplayType,screen);
window = XCreateSimpleWindow(eglNativeDisplayType, rootwindow, 0, 0, 400, 533, 0, 0, WhitePixel (eglNativeDisplayType, screen));
XMapWindow(eglNativeDisplayType, window);
native_window = window;
#else
const char *vendor = eglQueryString(egldisplay, EGL_VENDOR);
if (strstr(vendor, "Imagination Technologies"))
native_window = (EGLNativeWindowType)0;
else if (strstr(vendor, "AMD"))
native_window = (EGLNativeWindowType) open("/dev/fb0", O_RDWR);
else if (strstr(vendor, "Vivante")) //NEEDS FIX - functs don't exist on other platforms
{
#if (defined EGL_API_FB)
native_window = fbCreateWindow(eglNativeDisplayType, 0, 0, 0, 0);
#endif
}
else
{
printf("Unknown vendor [%s]\n", vendor);
return 0;
}
#endif
return native_window;
}
void fsl_destroywindow(EGLNativeWindowType eglNativeWindowType, EGLNativeDisplayType eglNativeDisplayType)
{
(void) eglNativeWindowType;
#if (defined EGL_USE_X11)
//close x display
XCloseDisplay(eglNativeDisplayType);
#endif
}
void GLInit (void)
{
static const EGLint s_configAttribs[] =
{
EGL_RED_SIZE, 5,
EGL_GREEN_SIZE, 6,
EGL_BLUE_SIZE, 5,
EGL_ALPHA_SIZE, 0,
EGL_SAMPLES, 0,
EGL_NONE
};
EGLint numconfigs;
printf("1");
eglNativeDisplayType = fsl_getNativeDisplay();
printf("2");
egldisplay = eglGetDisplay(eglNativeDisplayType);
printf("3");
eglInitialize(egldisplay, NULL, NULL);
printf("4");
assert(eglGetError() == EGL_SUCCESS);
printf("5");
eglBindAPI(EGL_OPENGL_ES_API);
printf("6");
eglChooseConfig(egldisplay, s_configAttribs, &eglconfig, 1, &numconfigs);
assert(eglGetError() == EGL_SUCCESS);
assert(numconfigs == 1);
printf("7");
eglNativeWindow = fsl_createwindow(egldisplay, eglNativeDisplayType);
assert(eglNativeWindow);
printf("8");
eglsurface = eglCreateWindowSurface(egldisplay, eglconfig, eglNativeWindow, NULL);
assert(eglGetError() == EGL_SUCCESS);
printf("9");
EGLint ContextAttribList[] = { EGL_CONTEXT_CLIENT_VERSION, 2, EGL_NONE };
eglcontext = eglCreateContext( egldisplay, eglconfig, EGL_NO_CONTEXT, ContextAttribList );
assert(eglGetError() == EGL_SUCCESS);
printf("10");
eglMakeCurrent(egldisplay, eglsurface, eglsurface, eglcontext);
assert(eglGetError() == EGL_SUCCESS);
}
void GLEnd (void)
{
printf("Cleaning up...\n");
eglMakeCurrent(egldisplay, EGL_NO_SURFACE, EGL_NO_SURFACE, EGL_NO_CONTEXT);
assert(eglGetError() == EGL_SUCCESS);
eglDestroyContext(egldisplay, eglcontext);
eglDestroySurface(egldisplay, eglsurface);
fsl_destroywindow(eglNativeWindow, eglNativeDisplayType);
eglTerminate(egldisplay);
assert(eglGetError() == EGL_SUCCESS);
eglReleaseThread();
}
int main (int argc, char **argv)
{
GLInit();
for( int i = 0; i < 100000; ++i)
{
glClear(GL_COLOR_BUFFER_BIT | GL_DEPTH_BUFFER_BIT); // Clear The Screen And The Depth Buffer
glClearColor (.0f, .0f, 1.0f, 1.0f);
eglSwapBuffers (egldisplay, eglsurface);
}
GLEnd();
}
Above code is stitched together from samples from GPU SDK.
I've built an image using Yocto (dylan branch) and build the meta-toolchain-qt (and qte).
Successfully managed to build above code ONLY FOR X11.
Issues i am facing:
1) if build for X11 and run app on the board, window shows, but it stays white, when it should be BLUE...doesn't update no matter what color i glClear to.
2) when compiling with FB, fbCreateWindow and etc don't get recognized, i.e. undefined reference to `fbCreateWindow' .... WHAT header contains these functions????
3) if even the basic samples don't work, how the hell is anybody supposed to build a GL application on this board?? --- more rhetorical than a real question, just frustrated here... what did i do wrong?
4) please show me a working tutorial or some code on how to get this EGL context initialized...i'm running at wit's end here...
Peter:
I have the Vivante OpenGL ES 2.0 samples building and running on a WandBoard Quad using the Yocto Dora release in FB mode and I have summarized the procedure I used on the WandBoard Google Groups forum. I have not tried the X11 mode yet. Did you get that to work?
yep...in the end, somebody did his/ber job and included good lib files into Yocto source. i could then compile and link to EGL succesfully with X11.