i.mx6 Yocto OpenGL ES 2 X11 (or FB)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 Yocto OpenGL ES 2 X11 (or FB)

i.mx6 Yocto OpenGL ES 2 X11 (or FB)

Hello!

Here's some CODE!!!

#include <iostream>

#include <stdio.h>

#include <assert.h>

#include <string.h>

#include <fcntl.h>

#include <malloc.h>

#include <math.h>

#include <stdlib.h>

//#define EGL_USE_GLES2

#include <GLES2/gl2.h>

#include <EGL/egl.h>

#include <GLES2/gl2ext.h>

#include <EGL/eglext.h>

#include <termios.h>

#include <unistd.h>

#include <fcntl.h>

#ifdef EGL_USE_X11

#include <X11/X.h>

#include <X11/Xlib.h>

#endif

EGLDisplay egldisplay;

EGLConfig eglconfig;

EGLSurface eglsurface;

EGLContext eglcontext;

EGLNativeWindowType eglNativeWindow;

EGLNativeDisplayType eglNativeDisplayType;

EGLNativeDisplayType fsl_getNativeDisplay()

{

  EGLNativeDisplayType eglNativeDisplayType = NULL;

#if (defined EGL_USE_X11)

  eglNativeDisplayType = XOpenDisplay(NULL);

  assert(eglNativeDisplayType != NULL);

#elif (defined EGL_API_FB)

  eglNativeDisplayType = fbGetDisplayByIndex(0); //Pass the argument as required to show the framebuffer

#else

  display = EGL_DEFAULT_DISPLAY;

#endif

  return eglNativeDisplayType;

}

EGLNativeWindowType fsl_createwindow(EGLDisplay egldisplay, EGLNativeDisplayType eglNativeDisplayType)

{

  EGLNativeWindowType native_window = (EGLNativeWindowType)0;

#if (defined EGL_USE_X11)

  Window window, rootwindow;

  int screen = DefaultScreen(eglNativeDisplayType);

  rootwindow = RootWindow(eglNativeDisplayType,screen);

  window = XCreateSimpleWindow(eglNativeDisplayType, rootwindow, 0, 0, 400, 533, 0, 0, WhitePixel (eglNativeDisplayType, screen));

  XMapWindow(eglNativeDisplayType, window);

  native_window = window;

#else

  const char *vendor = eglQueryString(egldisplay, EGL_VENDOR);

  if (strstr(vendor, "Imagination Technologies"))

  native_window = (EGLNativeWindowType)0;

  else if (strstr(vendor, "AMD"))

  native_window = (EGLNativeWindowType)  open("/dev/fb0", O_RDWR);

  else if (strstr(vendor, "Vivante")) //NEEDS FIX - functs don't exist on other platforms

  {

#if (defined EGL_API_FB)

  native_window = fbCreateWindow(eglNativeDisplayType, 0, 0, 0, 0);

#endif

  }

  else

  {

  printf("Unknown vendor [%s]\n", vendor);

  return 0;

  }

#endif

  return native_window;

}

void fsl_destroywindow(EGLNativeWindowType eglNativeWindowType, EGLNativeDisplayType eglNativeDisplayType)

{

  (void) eglNativeWindowType;

#if (defined EGL_USE_X11)

  //close x display

  XCloseDisplay(eglNativeDisplayType);

#endif

}

void GLInit (void)

{

  static const EGLint s_configAttribs[] =

  {

  EGL_RED_SIZE, 5,

  EGL_GREEN_SIZE, 6,

  EGL_BLUE_SIZE, 5,

  EGL_ALPHA_SIZE, 0,

  EGL_SAMPLES, 0,

  EGL_NONE

  };

  EGLint numconfigs;

  printf("1");

  eglNativeDisplayType = fsl_getNativeDisplay();

  printf("2");

  egldisplay = eglGetDisplay(eglNativeDisplayType);

  printf("3");

  eglInitialize(egldisplay, NULL, NULL);

  printf("4");

  assert(eglGetError() == EGL_SUCCESS);

  printf("5");

  eglBindAPI(EGL_OPENGL_ES_API);

  printf("6");

  eglChooseConfig(egldisplay, s_configAttribs, &eglconfig, 1, &numconfigs);

  assert(eglGetError() == EGL_SUCCESS);

  assert(numconfigs == 1);

  printf("7");

  eglNativeWindow = fsl_createwindow(egldisplay, eglNativeDisplayType);

  assert(eglNativeWindow);

  printf("8");

  eglsurface = eglCreateWindowSurface(egldisplay, eglconfig, eglNativeWindow, NULL);

  assert(eglGetError() == EGL_SUCCESS);

  printf("9");

  EGLint ContextAttribList[] = { EGL_CONTEXT_CLIENT_VERSION, 2, EGL_NONE };

  eglcontext = eglCreateContext( egldisplay, eglconfig, EGL_NO_CONTEXT, ContextAttribList );

  assert(eglGetError() == EGL_SUCCESS);

  printf("10");

  eglMakeCurrent(egldisplay, eglsurface, eglsurface, eglcontext);

  assert(eglGetError() == EGL_SUCCESS);

}

void GLEnd (void)

{

  printf("Cleaning up...\n");

  eglMakeCurrent(egldisplay, EGL_NO_SURFACE, EGL_NO_SURFACE, EGL_NO_CONTEXT);

  assert(eglGetError() == EGL_SUCCESS);

  eglDestroyContext(egldisplay, eglcontext);

  eglDestroySurface(egldisplay, eglsurface);

  fsl_destroywindow(eglNativeWindow, eglNativeDisplayType);

  eglTerminate(egldisplay);

  assert(eglGetError() == EGL_SUCCESS);

  eglReleaseThread();

}

int main (int argc, char **argv)

{

  GLInit();

  for( int i = 0; i < 100000; ++i)

  {

  glClear(GL_COLOR_BUFFER_BIT | GL_DEPTH_BUFFER_BIT);     // Clear The Screen And The Depth Buffer

  glClearColor (.0f, .0f, 1.0f, 1.0f);

  eglSwapBuffers (egldisplay, eglsurface);

  }

  GLEnd();

}


Above code is stitched together from samples from GPU SDK.

I've built an image using Yocto (dylan branch) and build the meta-toolchain-qt (and qte).

Successfully managed to build above code ONLY FOR X11.

Issues i am facing:

1) if build for X11 and run app on the board, window shows, but it stays white, when it should be BLUE...doesn't update no matter what color i glClear to.

2) when compiling with FB, fbCreateWindow and etc don't get recognized, i.e. undefined reference to `fbCreateWindow' .... WHAT header contains these functions????
3) if even the basic samples don't work, how the hell is anybody supposed to build a GL application on this board?? --- more rhetorical than a real question, just frustrated here... what did i do wrong?

4) please show me a working tutorial or some code on how to get this EGL context initialized...i'm running at wit's end here...

评论

Peter:

  I have the Vivante OpenGL ES 2.0 samples building and running on a WandBoard Quad using the Yocto Dora release in FB mode and I have summarized the procedure I used on the WandBoard Google Groups forum.  I have not tried the X11 mode yet.  Did you get that to work?

yep...in the end, somebody did his/ber job and included good lib files into Yocto source. i could then compile and link to EGL succesfully with X11.

I am looking for the OpenGL ES 2.0 code based on FB, which can be built and run in yocto enviornment(backend FB).

Could you provide the sample code ? Thanks.

无评分
版本历史
最后更新:
‎10-15-2013 04:37 PM
更新人: