i.MX51 EVK Board OpenCV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX51 EVK Board OpenCV

i.MX51 EVK Board OpenCV

OpenCV is a computer vision library originally developed by Intel. It is free for commercial and research use under the open source BSD license. The library is cross-platform. It focuses mainly on real-time image processing; as such, if it finds Intel's Integrated Performance Primitives on the system, it will use these commercial optimized routines to accelerate itself.


Application

OpenCV's application areas include:

* 2D and 3D feature toolkits 
* Egomotion estimation 
* Face Recognition 
* Gesture Recognition 
* Human-Computer Interface (HCI) 
* Mobile robotics 
* Motion Understanding 
* Object Identification 
* Segmentation and Recognition 
* Stereopsis Stereo vision: depth perception from 2 cameras 
* Structure from motion (SFM) 
* Motion Tracking

To support some of the above areas, OpenCV includes a statistical machine learning library that contains:

* Boosting 
* Decision Trees 
* Expectation Maximization 
* k-nearest neighbor algorithm 
* Naive Bayes classifier 
* Artificial neural networks 
* Random forest 
* Support Vector Machine

Installing OpenCV on i.MX 51 EVK Board running Ubuntu Linux

Assuming that you already have the Ubuntu Linux running on your board, you can use this wiki page to guide you to get your USB camera running on your system in order to use real time image processing features of this library.

In a brand new installation of Ubuntu some libraries is not installed by default, so you need to install them by your own hands (use synaptic to do that), here is the list of these libraries:

  1. libgtk2.0-dev
  2. libjpeg62-dev
  3. zlib1g-dev
  4. libpng12-dev
  5. libtiff4-dev
  6. libjasper-dev
  7. libgst-dev
  8. libgstreamer0.10-dev

If you already have some of those libraries installed, make sure that is the DEV version.

After installing those libraries you can download the stable OpenCV version here.

Install it following the procedure below:


1 - untar the opencv package

tar -xvzf opencv-1.1pre1.tar.gz  

2 - change to OpenCV folder

cd opencv-1.1.0  

3 - configure the installation enabling gstreamer and letting to compile demo apps later

./configure --with-gstreamer --disable-apps 


You will get the following results:

General configuration ================================================
      Compiler:                         g++
      CXXFLAGS:
      DEF_CXXFLAGS:             -Wall -fno-rtti -pipe -O3 -fomit-frame-pointer 
      PY_CXXFLAGS:               -Wall -pipe -O3 -fomit-frame-pointer 
      OCT_CXXFLAGS:             -fno-strict-aliasing -Wall -Wno-uninitialized -pipe -O3 -fomit-frame-pointer  

      Install path:                      /usr/local  

HighGUI configuration ================================================

      Windowing system --------------
      Use Carbon / Mac OS X:        no
      Use gtk+ 2.x:                        yes
      Use gthread:                         yes

      Image I/O ---------------------
      Use ImageIO / Mac OS X:       no
      Use libjpeg:                            yes
      Use zlib:                                yes
      Use libpng:                             yes
      Use libtiff:                               yes
      Use libjasper:                          yes
      Use libIlmImf:                          no
      
      Video I/O ---------------------
      Use QuickTime / Mac OS X:     no
      Use xine:                                no
      Use gstreamer:                        yes
      Use ffmpeg:                             no
      Use dc1394 & raw1394:     no
      Use v4l:                                   yes
      Use v4l2:                                 yes
      Use unicap:                             no
    
Wrappers for other languages ========================================= 
      SWIG Python                          no
      Octave                                    no
      
Additional build settings ============================================
      Build demo apps                      no

Now run make ...


4 - Build OpenCV

./make 

5 - Install OpenCV

./sudo make install 


if all steps above were executed properly, now you can compile the sample applications:

1 - change to samples/c directory

cd samples/c 

2 - change the build_all script mode to +x

chmod +x build_all.sh 

3 - run the script

./build_all.sh 


Now you can test. The results below were taken from the Laplacian filter sample processing in real-time images grabbed from an USB camera:

Laplace_filter.jpg
Laplacian filter with USB Camera capture device


Also, you can see how is it performance on a 3 windowed application performing color conversion and canny edge detection at the same time:

http://www.youtube.com/watch?v=w9yQgdABT7c

EOF !


ラベル(3)
評価なし
バージョン履歴
最終更新日:
‎09-10-2020 01:40 AM
更新者: