i.MX35 PDK Board NAND Flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX35 PDK Board NAND Flashing

i.MX35 PDK Board NAND Flashing

ATK (Advanced Toolkit)


ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here.


Using ATK

This section will describe the procedure to erase the flash memory and program the bootloader.

1 - Connect a serial cable between PC and i.MX board.

2 - Some hardware configurations (switches) must be done to flash the board.

Set red and cream switches as below: 
Switch SW5 -> 000000 
Switch SW4 -> 1000000


400px-Pdk_switch_program.jpg

{{Note|On SW5 and SW4, "1" means the keys selected towards the edge of the board.}


3 - Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit

IMX35_atk.jpg

Set the options: 
i.MX CPU -> i.MX35_TO2 
Device memory -> DDR2; 
Custom Initial File -> (keep it unmarked) 
Communication Channel -> Serial Port (Usually COM1)

If you are using TO1, Device Memory -> MDDR

4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO

Atk2.jpg

NAND Flash Erasing

1- Configure the Dip Switch of Personality Board:

Switch12345678
SW1OFFOFFOFFOFFN/AN/AN/AN/A
SW2ONOFFOFFONONOFFOFFOFF

2- Choose NAND model K9LAG08U8M

3- Continue the steps

Remember to select the checkbutton BBT (Back Block Table)


标记 (2)
评论

After I program the u-boot bin,what should I do ?How to set the switch to boot from the NAND FLASH?

Please use section 3.2 (Dip switch setup for boot modes) of "pdk2009_12_imx35_Linux_UG.pdf" in Linux
documentation package.

https://www.freescale.com/webapp/Download?colCode=IMX35_PDK0912_LINUXDOCS_BUNDLE&location=null&fpsp=...

thank you very much,I will try it.

在 2013-05-06 09:37:22,"Yuri Muhin" <admin@community.freescale.com> 写道:

|

|

|

|

i.MX35 PDK Board Flashing NAND

new comment by Yuri MuhinView all comments on this document

Please use section 3.2 (Dip switch setup for boot modes) of "pdk2009_12_imx35_Linux_UG.pdf" in Linux

documentation package.

https://www.freescale.com/webapp/Download?colCode=IMX35_PDK0912_LINUXDOCS_BUNDLE&location=null&fpsp=...

Reply to this email to respond to Yuri Muhin's comment.

|

|

Thank you for your advice.I have succeeded with your suggestion.

无评分
版本历史
最后更新:
‎09-10-2020 03:30 AM
更新人: