ATK (Advanced Toolkit) is a Windows software for programming the flash memory of i.MX boards. It can be downloaded here.
This section will describe the procedure to erase the flash memory and program the bootloader.
1 - Connect a serial cable between PC and i.MX board.
2 - Some hardware configurations (switches) must be done to flash the board.
Set red and cream switches as below: Switch SW5 -> 000000 Switch SW4 -> 1000000
{{Note|On SW5 and SW4, "1" means the keys selected towards the edge of the board.}
3 - Run ATK (1.6 or above) going to Start -> Programs -> AdvancedToolKit -> AdvancedToolKit
Set the options: i.MX CPU -> i.MX35_TO2 Device memory -> DDR2; Custom Initial File -> (keep it unmarked) Communication Channel -> Serial Port (Usually COM1)
If you are using TO1, Device Memory -> MDDR
4 - Click on Flash Tools to erase, program or dump the the flash memory and click GO
1- Configure the Dip Switch of Personality Board:
| Switch | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 |
| SW1 | OFF | OFF | OFF | OFF | N/A | N/A | N/A | N/A |
| SW2 | ON | OFF | OFF | ON | ON | OFF | OFF | OFF |
2- Choose NAND model K9LAG08U8M
3- Continue the steps
Remember to select the checkbutton BBT (Back Block Table)
After I program the u-boot bin,what should I do ?How to set the switch to boot from the NAND FLASH?
Please use section 3.2 (Dip switch setup for boot modes) of "pdk2009_12_imx35_Linux_UG.pdf" in Linux
documentation package.
thank you very much,I will try it.
在 2013-05-06 09:37:22,"Yuri Muhin" <admin@community.freescale.com> 写道:
|
|
|
|
i.MX35 PDK Board Flashing NAND
new comment by Yuri MuhinView all comments on this document
Please use section 3.2 (Dip switch setup for boot modes) of "pdk2009_12_imx35_Linux_UG.pdf" in Linux
documentation package.
Reply to this email to respond to Yuri Muhin's comment.
|
|
Thank you for your advice.I have succeeded with your suggestion.