Hi,
this is a smart server called Duckbill in a thumb-drive format based on the i.MX283. It's a really low cost solution usable with or without casing.
It is intended to be set up as a small home-server for automation purposes. It comes with Debian Linux as operation system but without any specific user programs.
The stick can be operated either at a USB power adaptor or at a USB port of your router.
Since Duckbill runs Linux you are totally free in software development.
The internal connectors can be used as UART, SPI, I2C, ADC or GPIO. So it's up to everyone to develop his own expansion board.
![Duckbill_Board_Top_n.gif Duckbill_Board_Top_n.gif](/t5/image/serverpage/image-id/45275i54D569BF6C1CA207/image-size/large?v=v2&px=999)
1. Duckbill without casing (top)
![Duckbill_Board_Bottom_n.gif Duckbill_Board_Bottom_n.gif](/t5/image/serverpage/image-id/45274iD73A345AC1AAB390/image-size/large?v=v2&px=999)
2. Duckbill without casing (bottom)
![Duckbill_n.gif Duckbill_n.gif](/t5/image/serverpage/image-id/45273i2C1BF2113E967B8F/image-size/large?v=v2&px=999)
3. Duckbill with casing
![Duckbill_Pins_Gehaeuse_n.gif Duckbill_Pins_Gehaeuse_n.gif](/t5/image/serverpage/image-id/45272i85FB9CF9F3CF3919/image-size/large?v=v2&px=999)
4. Duckbill for development purposes
![Duckbill_EnOcean_offen_n.gif Duckbill_EnOcean_offen_n.gif](/t5/image/serverpage/image-id/45271i98CB0F0FBB4A5772/image-size/large?v=v2&px=999)
5. Duckbill with integrated EnOcean module
If you want to know more about this product:
http://www.i2se.com/homeautomation.html