You already know. Your source code is one week old now, so please, update it (or should I say 'sync' it?)! Get used to update your BSP layers.
Is the name of file that determinates how a package should act. For example, the version, where it is the mainstream repo, how to build, install, link. etc.
For meta-fsl-arm the kernel recipes are under meta-fsl-arm/recipes-kernel/linux (take a look here meta-fsl-arm - Layer containing Freescale ARM hardware support metadata)
For meta-fsl-arm, there are 3 kernel recipes:
linux-fslc_3.8.bb --> kernel mainline (from kernel.org)
linux-imx_2.6.35.3.bb --> kernel from FSL, for imx5x and imx28
linux-imx_3.0.35.bb --> kernel from FSL for imx6
Take the linux-imx for imx6 as an example meta-fsl-arm - Layer containing Freescale ARM hardware support metadata
The recipe determinates:
In order to see where the source code is cloned from, you need to go to .inc file meta-fsl-arm - Layer containing Freescale ARM hardware support metadata
SRC_URI = "git://git.freescale.com/imx/linux-2.6-imx.git \
file://defconfig \
"
it´s from git.freescale.com. In addition, there is a defconfig file added on SRC_URI.
There is a defconfig file for every board, on every Linux revision. Some defconfigs are shared for more than one board (for example, every mx6 board), and some Linux version are not compatible for some boards (for example, imx53 is only compatible with 2.6.35).
During a bitbake linux-imx, a temp folder will be created under build/tmp/armv7-imx6....../linux-imx, with code from git, patches and defconfig. Then bitbake takes that defconfig and configure the kernel, built it, and deploy it.
So, in order to change the kernel configuration (make menuconfig) you must replace your defconfig file from meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6
Create the new defconfig
Copy it to meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6 (or the right folder for your board/kernel)
$ bitbake -c cleansstate linux-imx
$ bitbake linux-imx (if you want only the kernel image)
$ bitbake fsl-image-gui (if you want to generate a complete image using the new kernel)
$ bitbake -c menuconfig linux-imx
will generate a config file on tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r33.10/git/.config
$ bitbake -c menuconfig linux-imx
(change anything)
$ cp tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r33.10/git/.config ../sources/meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6/defconfig
$ bitbake -c cleansstate linux-imx
$ bitbake fsl-image-gui
The uImage will be under tmp/deploy/image
In order to replace only uImage binary into one ready sdcard:
$sudo cp tmp/deploy/image/uImage-imx6-XXX.bin /media/user/Boot imx6/uImage
In order to use kernel mainline instead of linux-imx. Please add the following code to your conf/local.conf
PREFERRED_PROVIDER_virtual/kernel = "linux-fslc"
Make sure the desired board is supported by kernel.org.
In order to take and build kernel mainline manually, please see https://community.freescale.com/docs/DOC-95017
It´s not a simple task, I know. Yocto is not the best tool for use to develop and customize kernel during development stage. It is easier to use an external toolchain (bitbake meta-toolchain). Once the kernel development, or customization, is done, the changes can be integrated in the Yocto so it is managed for production use.
I like to have a copy of kernel source code cloned on my machine directly from git.freescale.com, then I can re-configure it, rebuild it, apply some patches, make changes, and build it manually - any way I want it. So, I only change kernel using yocto when I know the bug and I know how to fix it, and I have the patch. (and this is the way I like to work)
Although this is how to configure (and even patch) kernel (if you want to patch kernel, follow the example in the recipes)
If you face any error, please, let me know. I tested the steps and it worked, but I´m using an Ubuntu machine, not a virtual machine (and I´m not sure how -c menuconfig will act in a virtual machine).
Go to Yocto Training - HOME
Not strictly part of the kernel but part of the OS is the init mechanism
To select systemd instead of sysvinit add the following to conf/local.conf
DISTRO_FEATURES_append = “ systemd”
VIRTUAL-RUNTIME_init_manager = “systemd”
Guys, you are awesome!
Thanks a lot for your comments
I finally got around to trying PREFERRED_PROVIDER_virtual/kernel = "linux-fslc" on a sabresd board but the resulting sdcard failed to complete its boot and instead stopped at:
Waiting for root device /dev/mmcblk1p2... mmc1: new high speed SDHC card at address b368 mmcblk0: mmc1:b368 SDC 3.72 GiB mmcblk0: p1 p2
The SDHC card seems to be detected at mmcblk0 instead of the required mmcblk1. There is probably something extra that I should have done when I changed to linux-fslc but I do not really understand it. Can you please explain
Have you plugged your SD on SD3 slot? That is the right slot.
Yes I am using SD3 near the HDMI
I have tried a number of things to try to get it working. The only combination that seems to work is to:
I haven´t tested sabrelite for a while now
But it does look like a bug.
Could you, please, submit a bug here:
https://bugzilla.yoctoproject.org/enter_bug.cgi?product=BSPs
It would be perfect if you could test with the newest u-boot-fslc (2013.10) before you report the bug. And please, don´t forget to select meta-fsl-arm
I was trying PREFERRED_PROVIDER_virtual/kernel = "linux-fslc" with meta-fsl-arm dylan core-image-minimal on a sabre-sd board
Do you still think it is a bug or does it work for you so is more likely something I have messed up?
Is mixing linux-fslc with u-boot-imx an unsupported combination?
Sorry for delay.
Do you have the bug number?
Please, make sure the bug is OK, and if it was the case, close it.
We are on final release cycle.
How i can rename the kernel version name?
Example:
rename 3.0.5-imx6-g324g56 to 3.0.5-imx6-my_name
in meta-fsl-arm we use LOCALVERSION
take a look here
http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/tree/recipes-kernel/linux/linux-imx.inc#n43
I tried to build the kernel 3.5.7 on Yocto Dora.(using imx6qsabreauto)
I added this code in my conf/local.conf
PREFERRED_VERSION_linux-imx_mx6 = "3.5.7"
I tried build with fsl-image-gui. There are no build errors.
But... I was met below problem.
.....
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading uImage
4737768 bytes read in 217 ms (20.8 MiB/s)
Booting from mmc ...
reading imx6q-sabreauto.dtb
43609 bytes read in 19 ms (2.2 MiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.5.7-1.0.0+3285970
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4737704 Bytes = 4.5 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Loading Kernel Image ... OK
OK
Using Device Tree in place at 18000000, end 1800da58
Starting kernel ...
(hang....)
I think machine id is not match between u-boot and kernel.
So, I used CONFIG_EARLY_PRINTK=y but there are no messages printed by kernel.
(UART number : 3)
I am having the same issue. I created a separate discussion (3.5.7 Kernel not booting).
Dear all,
I have addedd the fresscale-release-bsp so I can compile the 3.10.17 beta
So I tried to onfig it before to compile it: (taking from above istructions:)
"""""""""""""""""""""""""""""""""
$ bitbake -c menuconfig linux-imx (change anything)
$ cp tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.0.35-r33.10/git/.config ../sources/meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6/defconfig
$ bitbake -c cleansstate linux-imx
$ bitbake fsl-image-gui
""""""""""""""""""""""""""""""""
of course the directory for the 3.10.17 are different so my cp was:
cp tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/git/.config ../sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-kernel/linux/defconfig
I have some doubt on the destination dir, is it correct?I' not sure because in the recipes-kernel of the meta-fsl.bsp-release i don't have he subir "linux-imx-3.10.17/mx6" or similar,there is just the "recipes-kernel/linux" with the 3.10.17.bb file.... So where have I to put the defconfig file?
Omar
.
oh, I see.
So, please, create the folder and place the defconfig there.
create a folder here http://git.freescale.com/git/cgit.cgi/imx/meta-fsl-bsp-release.git/tree/imx/meta-fsl-arm/recipes-ker...
called linux-imx-3.10.17
meta-fsl-bsp-release does not receive patches
at least currently
:smileysad:
Another issue:
I compiled the kernel 3.10.17, my goal was to use it on sabrelite also ,but uboot says
"""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
file not found /boot/imx6q-sabrelite.dtb
...
... booting kernel from legacy Image at 10800000 ..
Image name: Linux-3.10.17 ....
Image type: ..
....
Staritng kernel ....
""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""""
then nothing more...
the /boot directory is the one of the rootfs? (so i have to update also the rootfs?)
why he is stucking ? in the menuconfig i activated the legacy AFLAGS.... shoudn't but anyway even if without dtb and dts?
Omar
Omar, are you subscribed to meta-freescale?
https://lists.yoctoproject.org/listinfo/meta-freescale
subscribe yourself and listen to the mailing list for a while.
I'm sure you're going to learn something there and when you fell comfortable you can start contribute to project :smileywink: