QSPI boot from IMX6UL board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QSPI boot from IMX6UL board

QSPI boot from IMX6UL board

1) nfs

I burn the uboot to board by mfgtool, then starting the kernel by nfs, when the board boot up, I set a) ipaddr and b)serverip, then I set the c)"setenv nfsroot /home/usuario/fsl-release-bsp/buildimx6q/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/rootfs", this is sample, you need choose correct folder for yours, this is for imx6q, d) set the mdt file,then run the netboot.

2) program uboot to the qspi, then boot from SD card

3) change the mfgtool to program uboot, kernel to the qspi

attched the ucl2.xml

setenv bootcmd 'run bootargsset; sf probe; sf read ${loadaddr} 0xA00000 0x600000; sf read ${fdt_addr} 0x800000 0x10000; bootz ${loadaddr} - ${fdt_addr}'

评论

hi  Joan Xie :

             能把你的文档和xml上传吗,我也需要试一下在demo板,uboot命令行有吗

unfortunately, we couldn't upload source code, so I couldn't complete my document, if I am aproved to upload it, I will attach it ASAP

无评分
版本历史
最后更新:
‎03-30-2018 06:42 AM
更新人: