When using SSI Slave Mode for ASRC_P2P function (https://community.freescale.com/docs/DOC-95342), the waveform of the converted 24bit data is abnormal(have some values between 0 and 1). When using SSI Master Mode, these abnormal data disappear. This patch shows how to enable SSI Master Mode based on ASRC_P2P patches.
Because SSI Master Mode uses fixed data width for LRCLK(32bits for each L or R), and the SSI Dual FIFO Mode is not supported for ASRC_P2P, the converted 16bit data is not well supported in this patch.
Suggestions:
If you want to convert the audio data to 16bit, you can use SSI Slave Mode; if you want to convert the audio data to 24bit, you can use SSI Master Mode.
Hi Lei Ge,
I had used above patch. It is for Normal Audio Playback (ASRC added in between PLAYBACK path & uses only one OUT CLK source i.e OUTCLK_SSI2_TX while IN CLK source is INCLK_NONE) and working perfectly fine!.
Now, I want to use ASRC in between Recording Path.I had tried following setup (taking above patch for reference):
1. Request DMA channel for P2P:
- DMA Request-SSI RX0
- P2P DMA request-ASRC RX1
Configured abvoe channel as Slave DMA channel. Input src is SSI-1 RX0, output dst is ASRC RX1 & direction is DMA_DEV_TO_DEV
2. Request DMA channel for P2M:
- DMA request-ASRC TX1
Configured abvoe channel as Slave DMA channel. Input src is ASRC TX1, output dst is MEMORY & direction is DMA_FROM_DEV
SSI is configured as SLAVE I2S device.
Configuratin of ASRC:
config.input_word_width = ASRC_WIDTH_24_BIT;
config.output_word_width = ASRC_WIDTH_24_BIT;
config.pair = iprtd->asrc_index; [ASRC_PAIR_A]
config.channel_num = channel; [2]
config.input_sample_rate = 48000;
config.output_sample_rate = 44100;
config.inclk = INCLK_SSI1_RX; [clk coming from SSI RX & its slave device]
config.outclk = OUTCLK_SSI2_TX; [clk coming from playback codec, SSI is master I2S (same as above patch)]
I had verified that both clock coming to ASRC.
My Result:
I received 'blank' data from MEMORY
Can you help me out, why i received 'blank' data. Or something is missing in above setup.
-Ankit.
Can you attach or share the patch in community?
Hi Lei Ge,
I am attaching patch at following locatin Audio LOST after ~10 hrs on i.MX 6Q for your reference. Please review it & give comments upon it.
Now, We got Audio lost after ~10 hrs after this attached patch. Issue explained in above link.
Note:
- We able to play smoothly till 10 hrs.
Hi Lei Ge,
Can you please give a comments over last attached patch here-Audio LOST after ~10 hrs on i.MX 6Q?
-Ankit.